FactoryTalk Optix Studio web editor
    You can use 
FactoryTalk Optix Studio
 in a web browser through FactoryTalk Hub
.Editor features support
      FactoryTalk Optix Studio web editor
 supports all FactoryTalk Optix Studio desktop editor
 features except for:
        - Save logs from theOutputtabs.
 - Edit NetLogic files.
 - OpenFactoryTalk OptixHelp.
 - Display paths in logs in theOutputtabs.
 - Add files and images by dragging and dropping them intoFactoryTalk Optix Studio web editor.
 - Restart the application at runtime by using the method.
 
Emulator features support
      FactoryTalk Optix Studio web editor
 emulator supports all features of FactoryTalk Optix Studio desktop editor
 emulator except for:
        - Control theWebBrowserobject in the runtime emulator.
 - Control thePDFViewerobject in the runtime emulator.
 - Control theVideoobject in the runtime emulator.
 - Control theWindowobject in the runtime emulator.
 
Provide Feedback