Develop a user-specific interface
    Provide personalized user experience and make certain interface areas accessible only for particular user groups.
Application example
The 
Admin Pane
 is only visible for logged-in administrators.

     NOTE: 
    
Download a sample project:
 UserSpecificInterface.zipPrerequisites
- Configure users and groups in the following way:User namePasswordGroupsAdmin1adminAdminsUser1userUsers
 
- To develop the project
 - Arrange the interface elements.
 - Save the project.
 

Select 
  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback