Create variables
    Create a variable that mimics raw data received from a controller and an analog variable that presents the controller data as a temperature unit.
- Create a variable that mimics raw data received from a controller:
- InProject view, right-clickModeland select .
 - Hover-over the variable, select, and enter
FromPLC. - InProperties, set theFromPLC (Int32)property value to60.
 
 - Create an analog variable that presents the controller data as a temperature unit:
- InProject view, right-clickModeland select .
 - Crete a dynamic link betweenAnalogValueand .For more information about dynamic links, see Create dynamic links.
 - Next to the dynamic link, select<None>and selectTemperature: degree Celsius.
 
 
Provide Feedback