Save and commit changes
    Save your progress and commit changes to the local version-control repository.
     TIP: 
    For more information about version control, including how to push changes into remote repositories, see Version control.
- From the toolbar, select.
 Save and Commit - If needed, in the prompt, selectOpen FactoryTalk Optix Studio optionsto configure your user name and email.The user name and email are needed to commit changes to the repository.
 - Enter a meaningful commit message.For example, enterConfigured quick start project.
 - SelectOK.
 
To see the commits history and restore the project to a commit, select 
 .
 View history
Commits history

Provide Feedback