Modify a model on a running gateway
Modify a model that is bound to applications running on the gateway. Redeploy the applications affected by the change to the models.
Modify a model when the gateway is either offline or online. To apply modifications made to the model while the gateway is offline, go online with the gateway and then download the current configuration to the gateway. To reconfigure and redeploy applications affected by the modified model, the gateway must be online.
TIP:
It is not possible to modify
FactoryTalk Smart Object
models in FactoryTalk Edge Gateway
. Modify FactoryTalk Smart Object
models in the project of the controller. After modifying a FactoryTalk Smart Object
model, repopulate the namespace from Data Sources
, then reconfigure and redeploy the dependent applications.To modify a model on a running gateway
- SelectData Flow>Models.
- SelectEdit
to modify the model. - SelectFinishto apply the modifications to the model.
- Review applications affected by the modified model.
- If currently offline, selectOnlineto go online with the gateway.FactoryTalk Edge Gatewaydisplays a green banner statingGateway Connection: Online.
- If prompted, selectDownloadto overwrite the running gateway configuration with the current modifications.
- Do these steps for applications affected by the modified model:
- SelectData Flow>Applicationsand then select an application from the tree view.
- SelectConfigureand select the modified model.
- Set the data collection properties for each bound tag and then selectSave.
- SelectDeployto send the updated model configuration to the application.
Provide Feedback