Application data flow

For each application,
Data Flow
displays this information when an application is deployed and
Enable Data Flow
is selected:
Data Flow
Description
Tag Name
This column displays the name of the tag sent to the application.
Data Source
This column displays the name of the data source associated to the tag.
Value
This column displays the current value of the tag.
Quality
This column displays the quality of the data sent.
Time
This column displays the date and time when the data refreshes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal