Quality codes for application data flow

When data flow is enabled for applications, a code indicating the quality of the data for each tag appears in the
Quality
column:
Code
Quality
Description
0
Bad [Non-Specific]
The value of the data is bad for an unknown reason.
4
Bad [Configuration error]
The value of the data is bad due to a server-specific problem with the configuration. For example, the tag was deleted from the configuration.
8
Bad [Not Connected]
No value is available at this time due to a disconnected input. The data source may not have provided the value.
12
Bad [Device Failure]
The data value is bad due to a device failure.
16
Bad [Sensor Failure]
The data value is bad due to a sensor failure.
20
Bad [Last Known Value]
Communications failed. The last known value is available.
24
Bad [Communication Failure]
Communications failed. The last known value is not available.
28
Bad [Out of Service]
The data value is bad. The tag may be off scan or locked.
32
Initializing
Initializing the data.
64
Uncertain [Non-Specific]
The value's quality is uncertain for an unknown reason.
65
Uncertain [Non-Specific] (Low Limited)
The value's quality is uncertain. The tag value pegged at some lower limit.
66
Uncertain [Non-Specific] (High Limited)
The value's quality is uncertain. The tag value pegged at some higher limit.
67
Uncertain [Non-Specific] (Constant)
The value's quality is uncertain. The tag value is a constant and cannot change.
68
Uncertain [Last Usable]
The value's quality is uncertain since the external source writing the value stopped returning values within an acceptable period. The data is considered stale.
69
Uncertain [Last Usable] (Low Limited)
The value's quality is uncertain since the external source writing the value stopped returning values within an acceptable period. The data is considered stale. The tag value pegged at some lower limit.
70
Uncertain [Last Usable] (High Limited)
The value's quality is uncertain since the external source writing the value stopped returning values within an acceptable period. The data is considered stale. The tag value pegged at some higher limit.
71
Uncertain [Last Usable] (Constant)
The value's quality is uncertain since the external source writing the value stopped returning values within an acceptable period. The data is considered stale. The tag value is a constant and cannot change.
80
Uncertain [Sensor Not Accurate]
The value's quality is uncertain. Internal diagnostics detected the sensor is uncalibrated.
81
Uncertain [Sensor Not Accurate] (Low Limited)
The value's quality is uncertain. The tag value pegged at some lower limit or internal diagnostics has detected the sensor is uncalibrated.
82
Uncertain [Sensor Not Accurate] (High Limited)
The value's quality is uncertain. The value pegged at some higher limit or internal diagnostics detected the sensor is uncalibrated.
83
Uncertain [Sensor Not Accurate] (Constant)
The value's quality is uncertain. The value is locked at a constant value or internal diagnostics detected the sensor is uncalibrated.
84
Uncertain [EU Exceeded]
The value's quality is uncertain. The value is outside the limits defined for the tag.
85
Uncertain [EU Exceeded] (Low Limited)
The value's quality is uncertain. The value is outside the lower limit defined for the tag.
86
Uncertain [EU Exceeded] (High Limited)
The value's quality is uncertain. The value is outside the higher limit defined for the tag.
87
Uncertain [EU Exceeded] (Constant)
The value's quality is uncertain. The value is outside the constant value defined for the tag.
88
Uncertain [Sub-Normal]
The value's quality is uncertain since the data is derived from multiple sources.
89
Uncertain [Sub-Normal] (Low Limited)
The value's quality is uncertain since the data is derived from multiple sources. The tag value has pegged at some lower limit.
90
Uncertain [Sub-Normal] (High Limited)
The value's quality is uncertain since the data is derived from multiple sources. The tag value pegged at some higher limit.
91
Uncertain [Sub-Normal] (Constant)
The value's quality is uncertain since the data is derived from multiple sources. The tag value is a constant and cannot change.
192
Good [Non-Specific]
The value's quality is good.
193
Good [Non-Specific] (Low Limited)
The value's quality is good. The tag value pegged at some lower limit.
194
Good [Non-Specific] (High Limited)
The value's quality is good. The tag value pegged at some higher limit.
195
Good [Non-Specific] (Constant)
The value's quality is good. The tag value is a constant and cannot change.
216
Good [Local Override]
The value's quality is good. The value was overwritten by a forced value.
217
Good [Local Override] (Low Limited)
The value's quality is good. The value was overwritten by a forced value. The tag value pegged at some lower limit.
218
Good [Local Override] (High Limited)
The value's quality is good. The value was overwritten by a forced value. The tag value pegged at some higher limit.
219
Good [Local Override] (Constant)
The value's quality is good. The value was overwritten by a forced value. The tag value is a constant and cannot change.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal