Monitor the data flow for a deployed application
Monitor the values of the data streaming from the gateway to the application. The gateway only monitors tags that have the
Data Collection
property set to On
.
TIP:
When enabled,
Data Flow
displays the values currently streaming through the gateway at the set data collection rates. Previous values are not retained in the gateway. To display all values streaming through the gateway at the set rates, select
Enable Data Flow
before deploying the application. Enabling data flow after deployment results in data only appearing in
Data Flow
at the next set collection rate (On change
or Update rate
).To monitor the data flow for a deployed application
- In the top-right corner of any view, selectOnlineto go online with the gateway.FactoryTalk Edge Gatewaydisplays a green banner statingGateway Connection: Online.
- SelectData Flow>Applications, and then select the required application from the tree view.
- SelectEnable Data Flow.
- FromData Flow, monitor the data flowing from the gateway to the application.
Provide Feedback