Applications

Applications in
FactoryTalk Edge Gateway
collect data from tags, models, or
FactoryTalk Smart Object
models and then send the data to the configured server or IoT device. For example, the
ThingWorx
application in
FactoryTalk Edge Gateway
sends data to the configured
PTC
ThingWorx
Foundation server.
FactoryTalk Edge Gateway
supports these applications:
  • Azure IoT Hub (Azure IoT Edge Runtime application will be available in the future release of FactoryTalk Edge Gateway distributed)
  • MSSQL
  • ThingWorx
    (standalone version only)
  • Test Client
  • MQTT
  • InfluxDB
In
FactoryTalk Edge Gateway
, monitor the values of live data flowing into the gateway.
Select
Error Log
to view errors for each deployed application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal