ThingWorx
template and shape mapping rules

FactoryTalk Edge Gateway
node properties map to properties inherited from a
ThingWorx
template or shape. If the node uses a
ThingWorx
template or shape but contains properties that are not in the
ThingWorx
template or shape,
FactoryTalk Edge Gateway
creates the corresponding properties on the target Thing.
To achieve correct property mapping across properties, set these properties in
ThingWorx
Composer.
  • Base Thing Template
    - Select
    Remote Thing
    .
    The
    Base Thing Template
    setting can be another
    ThingWorx
    template or shape if the underlying
    ThingWorx
    template or shape is based on a remote Thing.
  • Name
    - Name of the property. The name must match the
    FactoryTalk Edge Gateway
    property name exactly.
  • Base Type
    -
    Select the base type (data type). The base type must match the data type of the
    FactoryTalk Edge Gateway
    property.
    FactoryTalk Edge Gateway
    data type
    ThingWorx
    base type
    STRING
    STRING
    DINT
    Integer
    LINT
    Long
    REAL
    Number
  • Binding
    - Select
    Remotely Bound
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal