Back up FactoryTalk Edge Gateway configuration
FactoryTalk Edge Gateway
configuration
NOTE:
Applicable only for standalone version.
You can create a manual backup of your
FactoryTalk Edge Gateway
configuration.
TIP:
The configuration has password protection. This procedure uses the password you created when you first ran
FactoryTalk Edge Gateway
.
TIP:
When you move the backup data outside of the defined trust boundary, it is recommended to apply additional security controls (e.g. use password-protected package) to protect entire backup during transit.
To back up a
FactoryTalk Edge Gateway
configuration
TIP:
Before beginning this procedure, determine the location of your backup file. This example uses C:\fteg-ct\backup\resources.
- Launch the configuration tool.
- If prompted, upload the configuration from the gateway to resolve differences.
- Exit the configuration tool.
- Browse to the location of your resources directory. For example, C:\Program Files (x86)\Rockwell Software\FactoryTalk EdgC:\Program Files (x86)\Rockwell Software\FactoryTalk Edge Gateway\fteg-ct.
- Copy the resources directory from that location.
- Browse to your backup location. For example, C:\fteg-ct\backup\resources.
- Save the resources directory.
Provide Feedback