Test Client application
Use the Test Client application to test the connection to the gateway and make sure that your data sources and models are properly configured and sending the correct data.
The advantage of the Test Client application is that you do not need to configure an application for a server or IoT device to test the connection. The Test Client application displays live data streaming into the gateway when
Enable Data Flow
is selected.Provide Feedback