Modify an application on a running gateway
When
FactoryTalk Edge Gateway
is online with the gateway,modify the application by changing the application settings and Store and Forward settings. Modify the configuration of models and tags bound to the application.Other applications on the gateway continue to run and transmit data without interruption.
To modify an application on a running gateway
- SelectData Flow>Applications.
- SelectEdit
. - Modify the settings for the application and then selectSave.
- To modify the configured models and tags to deploy, selectConfigure.
- Update the configuration and selectSave.
- SelectDeployto send the modified configuration to the application.
Provide Feedback