Map property values to a
ThingWorx
template or shape

When a parent node uses a
ThingWorx
template or shape, by default, the properties of the node (DINT, REAL, LINT, STRING) map to properties inherited from the
ThingWorx
template or shape.
If the node uses a
ThingWorx
template or shape but contains properties that are not in the
ThingWorx
template or shape,
FactoryTalk Edge Gateway
creates the corresponding properties on the target Thing.
To map property values to a template or shape
  • In
    Properties
    , set these parameters:
    Template or Shape Property.
    Maps the value to properties inherited from a template or shape property. This is the default behavior.
    Thing Property.
    Maps the property to a new Thing property in ThingWorx Composer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal