ThingWorx Preview
ThingWorx
PreviewDuring configuration of a
ThingWorx
application, models selected from Models
appear in Preview
as a hierarchical structure of ThingWorx
Things. Preview
represents how the model appears in ThingWorx
.
TIP:
The Device Discovery model is not supported by
ThingWorx
application.Preview
displays a hierarchical structure of ThingWorx
Things using these icons:ThingWorx Icon | Description |
|---|---|
![]() | This icon represents a ThingWorx Thing Network . Thing Networks define the relationships between ThingWorx Things in a hierarchy.In FactoryTalk Edge Gateway , the Network represents the model name in the hierarchical structure. There is only one Network per model preview. |
![]() | This icon represents a ThingWorx Thing instance. Thing instances define the types of Things contained in a model.In FactoryTalk Edge Gateway , each Thing represents the parent node in the model hierarchy. |
![]() | This icon represents a ThingWorx Thing Property . Properties describe the data points directly related to a Thing .In FactoryTalk Edge Gateway , each Property represents a child node of a parent node in the model hierarchy. |
Provide Feedback