Configure and deploy an application
After adding an application, configure the models and tags to bind them to the application. Use the bound tags and models to access the information stored in the namespace of the data source.
Each model node and tag has an update rate and update type.
Deploy the application data after configuring the models and tags. During deployment of the new configuration, the existing configuration for the application is overwritten with the new one. Deploy the application any time after configuring the models and tags.
To configure and deploy an application
- In the top-right corner of any view, selectOnlineto go online with the gateway.FactoryTalk Edge Gatewaydisplays a green banner statingGateway Connection: Online.
- SelectData Flow>Applicationsand then select the application to configure from the tree view.
- SelectConfigure. See Data collection properties
- FromModels and Tags, chooseSelect
to add models or tags to the application configuration. - FromSelect Models or Tags, chooseModelsorTags.
- (optional) Filter the data appearing inSelect Models or Tags:
- Use the list to select specific models or data sources.
- Use the text box to filter the list of models or data sources.
- For tags, use the pull-down list to select specific types.
- Select the models or tags to add to the configuration and then selectSave.TIP:SelectClear Allto erase the selected models or data sources.
- Set the data collection properties for each tag.
- FromModels and Tags, select a tag.
- FromProperties, set theUpdate RateandUpdate Typefor the tag.
- SelectSave.
- FromModels and Tags, select the tags and models to bind them to the application and then selectSave. These tags and models that are deployed to the application.
- SelectDeployto send the current bound tags and models to the application.Are you sure you want to deploy following changes?displays theCurrent configurationandNew configurationfor the application. SelectDeployto send theNew configurationto the gateway.
Provide Feedback