Assign a ThingWorx template or shape to a node in a model
ThingWorx
template or shape to a node in a modelAssign a
ThingWorx
template or shape to a single node in a FactoryTalk Edge Gateway
model.To assign a
ThingWorx
template or shape to a node in a model- Select a single node or property.
- InProperties, set these parameters:
- . Select this checkbox to assign a singleThingWorxtemplateThingWorxtemplate to a Thing. By default, a template name appears as a placeholder in the input field. Change the template name to match the template name inThingWorx. To create a Thing, the template name inThingWorxandFactoryTalk Edge Gatewaymust correspond.
- Add. User can add unlimited shapes.ThingWorxshapes
- SelectAdd.
- SelectSave.
Provide Feedback