Supported Profiles and its Datapoints
Below is the list of profiles and its datapoints supported by Device Discovery model.
SN | Profiles | Datapoints |
1 | Point I/O Communications Adapter | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault |
2 | ControlLogix ControlNet Adapter | |
3 | CompactLogix ControlNet Adapter | |
4 | CompactLogix Communications Adapter | |
5 | Point I/O Module | |
6 | ControlLogix HART I/O Module | |
7 | ControlLogix I/O Module | |
8 | CompactLogix I/O Module | |
9 | HART Enabled I/O Module | |
10 | iTRAK 5730 | |
11 | Kinetix 5500 Servo Drive | |
12 | PowerFlex 7000 Drive | |
13 | SMC-50 Solid-State Smart Motor Controller | |
14 | SMC Flex Solid-State Smart Motor Controller | |
15 | ControlLogix DeviceNet Adapter | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Idle Mode, Node 00 Faults, Node 00 Faults, Node 01 Faults, Node 02 Faults, Node 03 Faults, Node 04 Faults, Node 05 Faults, Node 06 Faults, Node 07 Faults, Node 08 Faults, Node 09 Faults, Node 10 Faults, Node 11 Faults, Node 12 Faults, Node 13 Faults, Node 14 Faults, Node 15 Faults, Node 16 Faults, Node 17 Faults, Node 18 Faults, Node 19 Faults, Node 20 Faults, Node 21 Faults, Node 22 Faults, Node 23 Faults, Node 24 Faults, Node 25 Faults, Node 26 Faults, Node 27 Faults, Node 28 Faults, Node 29 Faults, Node 30 Faults, Node 31 Faults, Node 32 Faults, Node 33 Faults, Node 34 Faults, Node 35 Faults, Node 36 Faults, Node 37 Faults, Node 38 Faults, Node 39 Faults, Node 40 Faults, Node 41 Faults, Node 42 Faults, Node 43 Faults, Node 44 Faults, Node 45 Faults, Node 46 Faults, Node 47 Faults, Node 48 Faults, Node 49 Faults, Node 50 Faults, Node 4 Faults, Node 52 Faults, Node 53 Faults, Node 54 Faults, Node 55 Faults, Node 56 Faults, Node 57 Faults, Node 58 Faults, Node 59 Faults, Node 60 Faults, Node 61 Faults, Node 62 Faults, Node 63 Faults |
16 | ControlLogix EtherNet/IP Adapter | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Ethernet Interface Speed, Ethernet Link Status, Ethernet Duplex, Ethernet Auto-Negotiation Duplex and Speed, Ethernet Manual Setting Requires Reset, Ethernet Local Hardware Fault |
17 | CompactLogix EtherNet/IP Adapter | |
18 | Point I/O EtherNet/IP Adapter | |
19 | PowerFlex 40 Drive | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Output Current : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Output Voltage : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, DC Bus Volts : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Drive Temp : Value (Default), Percent (Default), Minimum, Maximum, Default, Units |
20 | PowerFlex 70 Drive | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Output Current : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Output Voltage : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, DC Bus Volts : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Motor Velocity Feedback : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Drive Temp Pct : Value (Default), Percent (Default), Minimum, Maximum, Default, Units |
21 | PowerFlex 400 Drive | |
22 | PowerFlex 700 Drive | |
23 | PowerFlex 523 Drive | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Output Current : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Output Speed : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Output Power : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Output Voltage : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Run Time : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Trip Fault, Fault Code, Fault Code (Default), Source Port Number, Fault Text |
24 | PowerFlex 525 Drive | |
25 | PowerFlex 753 Drive | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Drive Temperature : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Output Current : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Output Frequency : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Output Power : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Output Voltage : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Run Time : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Cabinet Fan Total Life, Cabinet Fan Elapsed Life, Cabinet Fan Remaining Life, Cabinet Fan Event Level, Heatsink Fan Remaining Life, Internal Fan Remaining Life, Motor Bearing Total Life, Motor Bearing Remaining Life, Machine Bearing Total Life, Machine Bearing Remaining Life, Port Number If Fault, Fault Code Port 0, Fault Code Port 10, Fault Code Port 11, Fault Code Port 13, Fault Code Port Other, Fault Code (Default), Source Port Number, Fault Text |
26 | PowerFlex 755 Drive | |
27 | PowerFlex 755T Drive | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, HeatSink Temp Pct : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Output Current : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Output Current Max Limit : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Output Frequency : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Output Power Max Limit : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Output Power : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Output Voltage : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Motor Bearing Total Life : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Motor Bearing Remaining Life : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Machine Bearing Total Life : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Machine Bearing Remaining Life : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Elapsed Run Time : Value (Default), Percent (Default), Minimum, Maximum, Default, Units, Pod Fan Elapsed Life, Pod Fan Remaining Life, Pod Fan Event Level, Input Bay Roof Fan Elapsed Life, Input Bay Roof Fan Remaining Life, Input Bay Roof Fan Event Level, Power Roof Fan Elapsed Life, Power Roof Fan Remaining Life, Power Roof Fan Event Level, Wiring Bay Fan Elapsed Life, Wiring Bay Fan Remaining Life, Wiring Bay Fan Event Level, Control Bay Roof Fan Elapsed Life, Control Bay Roof Fan Remaining Life, Control Bay Roof Fan Event Level, Heatsink Fan Remaining Life, Port Number If Fault, Fault Code Port 0, Fault Code Port 9, Fault Code Port 10, Fault Code Port 11, Fault Code Port 12, Fault Code Port 13, Fault Code Port 14, Fault Code Port Other, Fault Code (Default), Source Port Number, Fault Text |
28 | PowerFlex 755TM Bus Supply | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, DC Bus Voltage : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Elapsed Run Time : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Control Pod Fan Remaining Life, Input Bay Roof Fan Remaining Life, Power Bay Roof Fan Remaining Life, Wiring Bay Fan Remaining Life, Control Bay Roof Fan Remaining Life, Heatsink Temp Pct, AC Line Voltage : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,AC Line Current : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,AC Line Frequency : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Measured Real Power : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Measured Reactive Power : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Power Factor : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Current Limit : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,L0 Stirring Fan Remaining Life, L0 Heatsink Fan Remaining Life, L1 Heatsink Fan Remaining Life, L2 Heatsink Fan Remaining Life, L3 Heatsink Fan Remaining Life, L4 Heatsink Fan Remaining Life, L5 Heatsink Fan Remaining Life, L6 Heatsink Fan Remaining Life, L7 Heatsink Fan Remaining Life, L8 Heatsink Fan Remaining Life, L9 Heatsink Fan Remaining Life, Port Number If Fault, Fault Code Port 0 ICB, Fault Code Port 0 SFIB, Fault Code Port 13 Converter Control, Fault Code Port 14 PIOB, Fault Code Port 14 PLI, Fault Code Port 14 ACP, Fault Code Port Other, Fault Code (Default), Source Port Number, Fault Text |
29 | PowerFlex 755TM Inverter | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Elapsed Run Time : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Control Pod Fan Remaining Life, Power Bay Roof Fan Remaining Life, Wiring Bay Fan Remaining Life, Control Bay Roof Fan Remaining Life, Heatsink Temp Pct : Value (Default), Percent (Default), Minimum, Maximum, Default, UnitsOutput Voltage : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Output Current : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Output Frequency : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Output Power : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Output Power Max Limit : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Motor Bearing Total Life : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,Machine Bearing Total Life : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,M achine Bearing Remaining Life : Value (Default), Percent (Default), Minimum, Maximum, Default, Units,M0 Heatsink Fan Remaining Life, M1 Heatsink Fan Remaining Life, M2 Heatsink Fan Remaining Life, M3 Heatsink Fan Remaining Life, M4 Heatsink Fan Remaining Life, M5 Heatsink Fan Remaining Life, M6 Heatsink Fan Remaining Life, M7 Heatsink Fan Remaining Life, M8 Heatsink Fan Remaining Life, M9 Heatsink Fan Remaining Life, Port Number If Fault, Fault Code Port 0 ICB, Fault Code Port 0 SFIB, Fault Code Port Other, Fault Code (Default), Source Port Number, Fault Text |
30 | PowerFlex 6000T Drive | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, AC Line Freq, AC Line Voltage, Ctrl Pod Temp, Units, DC Bus Volts, Units, Output Current, Units, Output Freq, Units, Output Voltage, Units, V Ref Commanded, Units, Motor Voltage Feedback, Units, Output Power, Units, Output Current Max Limit, Output Freq Min Limit, Output Freq Max Limit, Output Power Max Limit, Output Voltage Max Limit, Port Number If Fault, Fault Code Port 0, Fault Code Port 10, Fault Code Port 12, Fault Code Port 13, Fault Code Port 14, Fault Code Port Other, Fault Code (Default), Source Port Number, Fault Text |
31 | PowerMonitor 500 | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Average L-N Voltage, Average L-L Voltage, Line 1 Current, Line 2 Current, Line 3 Current, Average Frequency, Real Power, Power Factor, Real Power Demand, Consumption, Alarm 1, Alarm 2, Alarm 3, Alarm 4 |
32 | PowerMonitor 1000 | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Average L-N Voltage, Average L-L Voltage, Average Current, Average Frequency, Imbalance (Voltage), Imbalance (Current), Real Power, Power Factor, Consumption, kW Demand, Projected kW Demand, Phase Loss V1, Phase Loss V2, Phase Loss V3, PT Primary |
33 | PowerMonitor 5000 | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Phase Loss V1, Phase Loss V2, Phase Loss V3, IEEE 1159 Voltage THD Alarm or IEEE 1159 Voltage THD Alarm Condition, IEEE1159 Current THD Alarm or IEEE 1159 Current THD Alarm Condition, Sag Indication, Swell Indication, Transient Indication, IEEE1159 Imbalance Condition Volts, IEEE1159 Imbalance Condition Current, Average L-N Voltage, Average L-L Voltage, Average Current, Average Frequency, Real Power, Power Factor Average THD-Voltage, Average THD-Current, Imbalance (Voltage), Imbalance (Current), Consumption, KW Demand, Projected KW Demand, V1_V2_V3_PT_Primary |
34 | Festo CPX-FB36 Ethernet/IP Adapter | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Module 0 Input Size, Module 0 Output Size, Module 0 Identity, Module 1 Input Size, Module 1 Output Size, Module 1 Identity, Valve, Output, Input, Analog, Undervolt, Short Circuit, Open Circuit, Other Device Name, Flow, Consumption, Pressure, Valve Shut Off Status, Air Saving Status |
35 | FactoryTalk Historian ME Series A | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Total CPU, Fault word value, Running, DataCollectionActive, DataTransferActive, SAFEMODE, BADTAG, NTPsyncProblem, ServiceNotRunning, IpAddress1, IpAddress2, IpAddress3, IpAddress4 |
36 | FactoryTalk Historian ME Series B | |
37 | PanelView 5310 | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Ethernet Interface Speed, Ethernet Link Status, Ethernet Duplex, Ethernet Auto-Negotiation Duplex and Speed, Ethernet Manual Setting Requires Reset, Ethernet Local Hardware Fault |
38 | PanelView 5500 | |
39 | PanelView 5510 | |
40 | Point I/O IO-Link Master Module | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault Channel (0 - 3) : Operational Mode, Rollup, Device Connection Fault, Configuration In Process, Device Configuration Failed, Key Failure, Short Circuit, Process Input Data Invalid, Low Power Fault, Output Limit Fault, No IO Sizes, Vendor ID, Rockwell Device ID, Device Name, Application Tag, 42JT Margin Low Alarm, 871C Margin Status, 871TM Margin Status, 42EF Margin Low Alarm, 42EF Proximity Alarm, 42AF Margin Low Alarm, 42AF Proximity Alarm, 871FM Margin Status, 871FM Margin Low Alarm, 871FM Proximity Alarm, 46DFA Margin Low Alarm, 45DMS Minimum Distance Alarm, 45DMS Low Signal Quality, 45PLA Low Margin, 46CLR Low Margin, 45CRM Local Teach Dial Position, 836P-D2xxxA Pressure, 836P-D2xxxB Pressure, 836P-D2xxxC Pressure, 836P-D1xxxA Pressure, 836P-D1xxxB Pressure, 837T Temperature, Temperature, |
41 | ArmorBlock IO-Link Master Module | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault Channel (0 - 7) : Operational Mode, Rollup, Device Connection Fault, Configuration In Process, Device Configuration Failed, Key Failure, Short Circuit, Process Input Data Invalid, Low Power Fault, Output Limit Fault, No IO Sizes, Vendor ID, Rockwell Device ID, Device Name, Application Tag, 42JT Margin Low Alarm, 871C Margin Status, 871TM Margin Status, 42EF Margin Low Alarm, 42EF Proximity Alarm, 42AF Margin Low Alarm, 42AF Proximity Alarm, 871FM Margin Status, 871FM Margin Low Alarm, 871FM Proximity Alarm, 46DFA Margin Low Alarm, 45DMS Minimum Distance Alarm, 45DMS Low Signal Quality, 45PLA Low Margin, 46CLR Low Margin, 45CRM Local Teach Dial Position, 836P-D2xxxA Pressure, 836P-D2xxxB Pressure, 836P-D2xxxC Pressure, 836P-D1xxxA Pressure, 836P-D1xxxB Pressure, 837T Temperature, Temperature |
42 | ControlLogix Controller | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Total CPU, Idle CPU, System CPU, Comms CPU, I/O CPU, Messaging CPU, Motion CPU, Safety CPU, Redundancy CPU, User Tasks CPU, Free I/O Memory, Free Logic Memory, Total I/O Memory, Total Logic Memory, I/O Memory Biggest Block Size, Logic Memory Biggest Block Size |
43 | CompactLogix Controller with EtherNet/IP | |
44 | CompactLogix Controller | |
45 | ControlLogix Controller with EtherNet/IP | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Control Utilization, Messaging Utilization, I/O Utilization, Ethernet Interface Speed, Ethernet Link Status, Ethernet Duplex, Ethernet Auto-Negotiation Duplex and Speed, Ethernet Manual Setting Requires Reset, Ethernet Local Hardware Fault, |
46 | ControlLogix Process Controller | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, Control Core % Usage, Comms Core % Usage, Packet Processing Core % Usage, ForceStatus_b0, ForceStatus_b1, LED Status, Minor Fault Count, MinorFaultBits_b4, MinorFaultBits_b6, MinorFaultBits_b9, MinorFaultBits_b10, Total Connections Count, Total Connections Current, I/O Connections Allowed, I/O Connections Current, Produced Connections Allowed, Produced Connections Current, Consumed Connections Allowed, Consumed Connections Current, MSG Current Count, MSG Max Count |
47 | E1 Plus Electronic Overload Relay | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault |
48 | E3 Plus Solid-State Overload Relay | |
49 | E300 Electronic Overload Relay | |
50 | Stratix 5400 Managed Ethernet Switch | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, SFP Invalid, CDP mismatch, MAC address flap, Security violation, Internal Temperature, Major Output Alarm Relay Event, Minor Output Alarm Relay Event, Alarm Input 1 Event, Alarm Input 2 Event, Alarm Input 3 Event, Alarm Input 4 Event, Active Faults, IOS Release, Switch Uptime, Total Bandwidth Utilization, PTP Is Enabled, PTP Is Synchronized, Number Of Ports, Port #26 Utilization, Port #25 Utilization, Port #24 Utilization, Port #23 Utilization, Port #22 Utilization, Port #21 Utilization, Port #20 Utilization, Port #19 Utilization, Port #18 Utilization, Port #17 Utilization, Port #16 Utilization, Port #15 Utilization, Port #14 Utilization, Port #13 Utilization, Port #12 Utilization, Port #11 Utilization, Port #10 Utilization, Port #9 Utilization, Port #8 Utilization, Port #7 Utilization, Port #6 Utilization, Port #5 Utilization, Port #4 Utilization, Port #3 Utilization, Port #2 Utilization, Port #1 Utilization, Card Present, Card Corrupt, Card File(s) Corrupted, IOS Unsynchronized, Configuration Unsynchronized, Sync Failed |
51 | Stratix 5410 Managed Ethernet Switch | |
52 | Stratix 5700 Managed Ethernet Switch | |
53 | Stratix 8000 Managed Ethernet Switch | Fault Bits, Minor Recoverable Fault, Minor Unrecoverable Fault, Major Recoverable Fault, Major Unrecoverable Fault, SFP Invalid, CDP mismatch, MAC address flap, Security violation, Internal Temperature, Major Output Alarm Relay Event, Minor Output Alarm Relay Event, Alarm Input 1 Event, Alarm Input 2 Event, Alarm Input 3 Event, Alarm Input 4 Event, Active Faults, IOS Release, Switch Uptime, Total Bandwidth Utilization, PTP Is Enabled, PTP Is Synchronized, Number Of Ports, Port #26 Utilization, Port #25 Utilization, Port #24 Utilization, Port #23 Utilization, Port #22 Utilization, Port #21 Utilization, Port #20 Utilization, Port #19 Utilization, Port #18 Utilization, Port #17 Utilization, Port #16 Utilization, Port #15 Utilization, Port #14 Utilization, Port #13 Utilization, Port #12 Utilization, Port #11 Utilization, Port #10 Utilization, Port #9 Utilization, Port #8 Utilization, Port #7 Utilization, Port #6 Utilization, Port #5 Utilization, Port #4 Utilization, Port #3 Utilization, Port #2 Utilization, Port #1 Utilization |
Provide Feedback