Gateway Status

The
Gateway Status
displays data about the computer running
FactoryTalk Edge Gateway
and licensing information:
Data
Description
Total Memory
The total amount of RAM installed in the computer running the gateway.
Free Memory
The amount of RAM currently available in the computer running the gateway.
CPU
The percentage of the central processing unit (CPU) that
FactoryTalk Edge Gateway
currently uses.
Licensed Tags
The total number of licensed tags that all deployed applications use. If multiple applications use a tag, the tag is only counted once.
Maximum Licensed Tags
The maximum number of licensed tags available (100, 500, 2500, or 10000) based on the tag activation in use.
License Status
Displays the current license status:
  • Normal (expires mm/dd/yyyy)
  • Normal (Gold Master) (expires mm/dd/yyyy)
  • In grace period (x.y days remaining)
  • Grace period expired
  • Missing
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal