Start, stop, and pause a driver

Start, stop, and pause gateway drivers as needed. Pause a driver to stop incoming or outgoing data. The paused driver still exists on the gateway. Stop a driver to remove it from the gateway. The stopped driver is still available in the gateway configuration. You cannot stop a driver used by a running application.
To start, stop, and pause a driver
  1. Select
    Data Flow
    >
    Data Sources
    .
  2. From
    Define Drivers
    :
    • Select
      Run
      to start the driver.
    • Select
      Pause
      to pause the driver.
    • Select
      Stop
      to stop the driver.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal