EtherNet/IP (CIP) driver settings

The EtherNet/IP (CIP) driver enables communication between
FactoryTalk Edge Gateway
and data sources using a
CIP
network. When adding an EtherNet/IP driver to the gateway, configure these settings:
EtherNet/IP driver settings
Description
Driver Name
Defines the driver name.
Driver IP Address
Displays the Ipv4 address to use for
CIP
communication.
Driver Default Gateway IP Address
Displays the default gateway Ipv4 address to use for
CIP
communication. This setting is related to the
Driver IP Address
.
ADVANCED
Driver IpV4 Net Mask
Displays the Network IPv4 mask to use for
CIP
communication.
TIP:
If the computer where CIP adapter is running has multiple network interfaces, i.e. multiple IP addresses, ensure that the Driver IP Address and Driver Default Gateway IP Addess are configured correctly. That is, CIP adapter is 'sitting' on the same network as the target CIP devices.
Example:
Your computer have two network interfaces (i) 10.70.136.110, (ii) 192.168.1.10 and you want to communicate with CIP device available at 192.168.1.20, then the Driver IP Address must be set to 192.168.1.10.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal