Delete a model

Delete a model to remove it from the list of available models. It is only possible to delete a model that an application has not configured for use.
To delete a model
  1. Perform one of these actions:
    • Select
      Data Flow
      >
      Models
      .
    • Select
      Data Flow
      and then under
      Organize
      , select
      Configure
      .
  2. (optional) Filter the list of models.
  3. Select the models to delete.
  4. Select
    Delete
    .
  5. Select
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal