Add a driver
Drivers enable communication between the gateway and data sources. Add drivers to configure data collection paths for data sources and
FactoryTalk Smart Object
instances. Go Online
to add a driver.By default, an EtherNet/IP (CIP) driver is installed with
FactoryTalk Edge Gateway
.To add a driver
- SelectData Flow>Data Sources.
- FromDefine Drivers, selectAddto add a driver to the gateway.
- FromSelect Driver, select the driver type to configure:
- FactoryTalk Live Data (FTLD)
- EtherNet/IP (CIP)
- OPC Data Access (DA) (For standalone version only)
- KEPServer Enterprise (OPC DA) (For standalone version only)
- SelectNext.
- Enter theDriver Nameand define the
- The name must contain only letters, numbers, and hyphens.
- The settings differ for each driver type.
- ForOPC Data AccessandKepwaredrivers, selectAddto configureCREDENTIALS FOR SERVERS THAT WILL BE ACCESSED. These drivers support more than one instance of credentials.
- Select each credential and enter a value for theServer Identifier,Domain, andSystem username, andSystem password.
- SelectSave.
Provide Feedback