Bind tags to a model

Tags are elements of information from your data source. After adding a model and staging tags, associate tags to elements (nodes and properties) in the model.
TIP:
Tags are automatically bound in
FactoryTalk Smart Object
models.
To bind a tag to a model
  1. Perform one of the actions:
    • Select
      Data Flow
      >
      Models
      .
    • Select
      Data Flow
      and then under
      Organize
      , select
      Configure
      .
  2. Select
    Edit
    next to a model.
  3. (optional) Filter the list of tags.
  4. Perform one of these actions:
    • To select and bind multiple tags, under
      Tags
      , select the tags to associate to the node or property and then select
      Bind
      . The tags appear underneath the top-level node.
    • Select a tag, select a node or a property and then select
      Bind
      .
    • Drag and then drop a tag on a node or a property.
  5. Select
    Save
    .
    TIP:
    To unbind tags from a model, select the tags in the model and then select
    Unbind.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal