Data Egress

Data egress is implemented as applications in
FactoryTalk Edge Gateway
that have store and forward capabilities. Use applications to configure pathways that deliver contextualized data to the destination system. Data analysis or machine learning data preparation is executed at the destination system using your preferred analytics engine.
FactoryTalk Edge Gateway
supports these destination systems:
  • Azure IoT Hub (Azure IoT Edge Runtime will be available in a future release of distributed)
  • MSSQL
  • ThingWorx®
    (Available in the future release of distributed version)
  • MQTT
  • InfluxDB
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal