Data Ingress
Data ingress is implemented as data sources in
FactoryTalk Edge Gateway
. Data sources allow an OT engineer to identify data critical for analysis. Use FactoryTalk Edge Gateway
to configure a pathway to collect data from these sources:- Studio 5000 Logix Designerproject file (.acd)
- Studio 5000 Logix Designercontroller
- FactoryTalk® Live Datashortcut
- Drive/IMC device
- OPC DA device (standalone version only)
- KEPServer Enterprisedevice for third-party-data connectivity (standalone version only)
Provide Feedback