Data In

Data In
displays information about data sources flowing into the gateway:
Column
Description
Name
The name of the configured data source.
Driver
The name of the driver defined for the data source. The driver displays one of these statuses:
  • The driver is stopped.
  • The driver is paused.
  • The driver is running.
Collection Path
The collection path defined for the data source. The collection path displays one of these statuses:
  • The collection path is inactive.
  • The collection path is active.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal