Edit a model

Edit models at any time. Redeploy the applications to see the changes.
TIP:
FactoryTalk Smart Object
models are not editable.
To edit a model
  1. Perform one of these actions:
    • Select
      Data Flow
      >
      Models
      .
    • Select
      Data Flow
      and then under
      Organize
      , select
      Configure
      .
  2. Select
    Edit
    next to a model.
  3. Edit the model.
  4. Select
    Save
    .
  5. Review and redeploy any dependent applications.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal