Activation and Licensing - Distributed Version

FactoryTalk Edge Gateway distributed is bundled with FactoryTalk Edge Manager, and it is licensed through entitlements available in FactoryTalk Hub.
The number of available tags depends on the selected catalog, specifically the type of node included in the catalog.
A Type 1 Node includes 100 tags added to the available tag pool, while a Type 2 Node includes 500 tags added to the pool. It is possible to add an additional 1,000 tags separately.
Please refer to the https://commerce.rockwellautomation.com/rockwell/en/USD/login for more information on the bundle/toolkit catalogs.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal