Add a data source from a FactoryTalk Live Data Shortcut

Add data sources from
FactoryTalk Live Data
to populate a namespace and collect data from data tags. The data source is also a shortcut to these source types: HMI TagDb, OPC DA server, OPC UA server, and
FactoryTalk® Linx
shortcut.
The
FactoryTalk Live Data Shortcut
data source is compatible with the
FactoryTalk Live Data
driver.
To add a data source from a
FactoryTalk Live Data
shortcut
  1. Select
    Data Flow
    >
    Data Sources
    , and from
    Configure Data Sources,
    add a data source.
    • To add the first data source, select
      Add Data Sources
      .
    • To add a subsequent data source, select
      Add
      .
  2. Enter the name
    and then from
    Data Browse Path Type,
    select
    FactoryTalk Live Data Shortcut
    .
    • The name must contain only letters, numbers, and hyphens.
  3. From
    Driver for browsing,
    select the
    FactoryTalk Live Data
    driver.
  4. Select a network or local path and enter the browse path.
  5. (optional) To automatically generate the namespace, select
    Auto-populate namespace
    .
  6. Perform one of these:
    • Select
      Use browse path for data collection
      .
    • From
      Driver for Collection
      , select the
      FactoryTalk Live Data
      driver for the data collection path and enter the collection path.
  7. Select
    Save
    to add the data source.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal