Naming rules for models

Nodes of models mapped to applications must follow these naming rules:
  • Names must be unique for each model node located under the same parent level. For example, each property node under a parent node must use a unique name. The same name can be used for a property node located under a different parent node.
  • Names are mandatory.
  • Names are case insensitive.
  • Names are limited to 40 Unicode characters and can be alphanumeric; special characters are not supported.
  • Spaces and periods are supported, but not at the beginning or end of names.
  • Underscores are supported anywhere in the names.
Additional naming rules for
ThingWorx
applications
Nodes of models mapped to
ThingWorx
applications follow the naming rules as well as these additional rules:
  • The name cannot be the reserved keyword
    me
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal