Data sources
From
Data Sources
, first define drivers and then configure data sources. Drivers define the communication method used by FactoryTalk Edge Gateway
to collect data from data sources. Configure data sources to populate a namespace and collect data from data tags, models, and
FactoryTalk Smart Object
instances. FactoryTalk Smart Object
instances require an offline Studio 5000 Logix Designer
project file (.acd) to populate the namespace and an EtherNet/IP driver for data collection.Provide Feedback