Add nodes to a model
To build a model, add nodes or properties to create a hierarchical relationship between the elements of information.
To add nodes or properties to a model
- Perform one of these actions:
- SelectData Flow>Models.
- SelectData Flowand then underOrganize, selectConfigure.
- SelectEdit
next to the model.
- UnderModels, selectAdd Node.
- Type a name for the root node and pressEnter.
- To add a child node, right-click the parent node, selectAdd Child,and then selectNode.
- To add a child property under a node, right-click the parent node, selectAdd Child, and then selectProperty.
- Type the name of the child node or property and then pressEnter.
- To change the hierarchy, drag and then drop the nodes or properties.
- To move a node to the highest level, right-click the node and then selectMove to Root.
- To rename a node or property, right-click the node or property and then selectRename. Type a new name.
Provide Feedback