- Getting started
- Using the software
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Create an object type
Create an object type so that you can create instances of that type to show different values at runtime. Create a type in
Type view
.- When you create an object type, the original object from which you create the type becomes an instance of the new type.
- FromProject view, drag an object into a folder inType view.
The new object appears in
Type view
and the object name is appended with (type)
. The new type also appears in the same folder in Project view
.Provide Feedback