Create a converter type

Create a converter type and then use a converter instance to transform values in advanced dynamic links.
  1. In
    Project view
    , right-click
    Converters
    and select
    New
    Converter
    .
  2. (optional) Next to the converter object, select
    Edit
    to rename the converter.
  3. In
    Properties
    set the converter property values.
Use the converter type instance to transform values in advanced dynamic links. See Create a complex dynamic link.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.