View alarms in standard time zone

To view alarms in the standard time zone, you can display alarms events in the
Alarm Grid
and
Alarm History Grid
in the standard UTC time zone. Configure the time zone for the grid object in
Template Libraries
.
  1. Select
    Template Libraries
    .
  2. In
    Template Libraries
    , select
    Widgets
    .
  3. Drag
    Alarm grid
    or
    Alarm history grid
    from
    Widgets
    to the desired node in the
    UI
    folder.
  4. In
    Template Libraries
    , select
    Close
    .
  5. In
    Project view
    , expand the alarm grid and select
    AlarmsDataGrid
    .
  6. in
    Properties
    , expand
    Timestamp
    .
  7. In the
    Text
    property, right-click
    Complex Dynamic Link
    and then select
    Reset value
    .
  8. Select
    Change Dynamic Link
    .
  9. In the Dynamic Links window, configure either:
    • Alarm Grid
      . Expand
      Aliases
      , select
      {Item}[…]
      AlarmCondition
      , and then select the
      Time
      variable.
    • Alarm History Grid
      . Expand
      Aliases
      , select
      {Item}[…]
      PointedNode
      , and then select
      LocalTime
      . After
      LocalTime
      , select
      Edit
      and then type
      Time
      .
  10. Choose
    Select
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.