Edit or synchronize the imported tags

Synchronize imported tags to update their data types, names, and structures.
  1. To synchronize the imported tags
  2. In
    Project view
    , under a
    Communication station
    , double-click
    TagImporter
    .
    The editor opens in a separate tab and shows the status of each controller tag in the project.
  3. Make any necessary edits to the tags.
  4. Select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.