Create an object from a type

Create an object from a type. The new object is automatically of the same type.
  1. From
    Type view
    , double-click the folder with the category of objects.
  2. Drag the desired object type and into a folder or object in
    Project view
    .
The new object appears in
Project view
with the name appended with
(type)
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.