Edit the imported nodes at design time

Remove imported nodes and import new nodes.
Prerequisites
  1. To edit the imported nodes at design time
  2. In
    Project view
    , double-click an OPC UA client.
  3. In the editor, clear of the nodes to remove.
  4. Select the nodes  to add.
  5. Select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.