Configure panel types

Configure panel types to distribute interface elements over multiple pages in the application.
  1. In
    Project view
    , right-click
    UI
    and select
    New
    Folder
    .
  2. Hover-over
    NewFolder1
    , select
    Edit
    , and enter
    Pages
  3. Right-click
    Pages
    and select
    New
    Containers
    Panel
    .
    Panel1 (type)
    appears under
    Pages
    .
  4. Hover-over
    Panel1 (type)
    , select
    Edit
    , and enter
    Page
    .
  5. Set
    Width
    to
    1060
    and
    Height
    to
    500
    .
  6. Set
    Left margin
    , and
    Right margin
    to
    10
    .
  7. Right-click
    Pages
    and select
    New
    Pages
    Page
    four times.
    Page1 (type)
    ,
    Page2 (type)
    ,
    Page3 (type)
    , and
    Page4 (type)
    are created. Each
    Page# (type)
    inherits its properties from
    Page (type)
    .
    TIP: Create consistent user interfaces by inheriting properties from parent object types. For example, if you want to change
    Page1 (type)
    ,
    Page2 (type)
    ,
    Page3 (type)
    , and
    Page4 (type)
    margins, edit the margin properties of
    Page (type)
    . The modification will propagate to each
    Page# (type)
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.