Delete a method from an event

Delete a method from an event to no longer have the event perform that method.
Delete all of the methods from an event to delete the event.
  1. In
    Project view
    , select an object.
  2. In
    Properties
    under
    Events
    , expand the event.
  3. After the method to delete, select
    Delete
    .
The method is removed from the event.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.