Export translated strings to a CSV file

Export strings to use in the strings another project and help prevent having to recreate and translate the strings. Export translated strings to a CSV file using the predefined script in the template library.
  1. In the main toolbar, select
    Template Libraries
    .
  2. Select
    Scripts
    .
  3. Under
    Components
    , drag
    Translations Importer and Exporter
    into the project node or
    Translations
    folder.
  4. In
    Template Libraries
    , select
    Close
    .
  5. With
    Import and Export Translations
    selected, in
    Properties
    , in
    CSVPath,
    browse to select the .CSV file.
  6. In
    CharacterSeperator
    , select the separator.
  7. In
    Project view,
    right-click
    Import and Export Translations
    and then select
    Execute ExportTranslations
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.