Event types

Projects include predefined events and may include custom events.

Predefined events

Some objects contain predefined events. For example, a
Button
object contains a predefined
MouseClick event
that triggers an associated method when you select the button at runtime.
The
Events
pane lists the predefined events for an object.

Custom events

Custom events include configurable change events that occur at runtime when the value of a variable changes. For more information, see:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.