OPC UA and ODBC database data types

Data types map
FactoryTalk Optix
data type
Microsoft®
SQL Server data type
MySQL data type
Data type returned by a queried SQL database
Boolean
BIT
BIT(1)
Boolean
Integer
BIGINT
BIGINT
Int64
UInteger
BIGINT
BIGINT
Int64
byte
SMALLINT
SMALLINT UNSIGNED
Int16
SByte
SMALLINT
TINYINT
Int16
Int16
SMALLINT
SMALLINT
Int16
UInt16
INT
MEDIUMINT UNSIGNED
Int32
Int32
INT
INT
Int32
UInt32
BIGINT
BIGINT UNSIGNED
Int64
Int64
BIGINT
BIGINT
Int64
UInt64
BIGINT
BIGINT UNSIGNED
Int64
Float
REAL
FLOAT
Double
Double
FLOAT
DOUBLE
Double
DateTime
DATETIME
DATETIME(3)
DateTime
String
TEXT
TEXT
String
NodeId
VARBINARY (max)
BLOB
NodeId
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.