Global methods for variables

These global methods modify the values of variables.

Increment method

This method increases the value of a variable.
Input arguments
Argument
Description
VariableToModify
Variable for which to increment the value
Delta
Value of increase of a variable
ArrayIndex
(Only for array) Cell to modify

Set method

This method sets the value of a variable.
Input arguments
Argument
Description
VariableToModify
Value to modify
Value
Value to set
ArrayIndex
(Only for array) Cell to be modified

Toggle method

This method alternates the value of a Boolean variable.
Input arguments
Argument
Description
VariableToModify
Variable for which to alternate the value
ArrayIndex
(Only for array) Cell to modify
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.