Add a driver

Communication drivers allow the communication device installed in a computer to communicate with the network it is attached to. You must configure the driver on the computer that the project will run on.
To add a driver
  1. From the
    Communication Setup
    editor or the
    Communications
    tab in the
    FactoryTalk Administration Console
    or
    FactoryTalk View Studio
    , right-click on the device shown at the root, and click
    Add Driver
    .
  2. In the
    Add Driver Selection
    dialog box, the available drivers will appear. Select the driver you want to add, and click
    OK
    .
    TIP:
    If you are using the
    FactoryTalk Linx
    Instance02 Server, you can only add
    Ethernet
    drivers.
    Local
    FactoryTalk View SE
    or
    FactoryTalk View ME
    application doesn't support
    FactoryTalk Linx
    Instance02 Server.
  3. From the applicable driver properties dialog box, enter the settings and click
    OK
    .
  4. After you add the driver, right-click on the driver and then click
    Start Browsing
    to populate the driver with devices.
    TIP:
    • Tip: If you are adding a driver via an Ethernet network, from the
      Communications Setup
      editor, right-click on the network shown, then select
      Start Browsing
      to populate the driver with devices.
    • Some Ethernet devices may not support the browse protocol used by
      FactoryTalk Linx
      on Ethernet. If the devices you expect to appear during the browse do not display, right-click the network and click
      Add Device
      to manually add the device to the Ethernet network of the workstation. Before you add a device manually, you must register it using the Device Description File Installation Tool.
    • The DHCP Host name or IP Address lists / range configuration for the Ethernet driver configured in the
      FactoryTalk Linx
      Network Browser
      control embedded within
      Studio 5000
      can be browsed in either the
      Communications Setup
      editor or the
      Communications
      tab in the
      FactoryTalk Administration Console
      but can only be modified from with the embedded
      Network Browser
      control.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal