DH+ Properties dialog box settings

The following are the settings for the
DH+
Driver Properties
dialog box.
Setting
Description
Name
Used to view or adjust the name of the driver. The default name is the 1784-PKTX or a
DH+
driver. If you change the name, you must enter a name that is unique across the entire topology, and is limited to 255 characters. The new name shows in the communications tree.
Station Number
Used to enter the Station Number for the driver. The Station Number must be unique to this network. No other devices on the network can be assigned this address. All packets sent to this station address are forwarded to
FactoryTalk Linx
. Available station numbers are 0 to 77 decimal (default is 0).
Jumper ID
Displays the 1784-PKTX card number, which is set using the jumpers on the card. This ID must match the value set with the jumpers on the 1784-PKTX card. Available jumper IDs are 0, 1, 2, and 3 (default is 0).
Baud
Used to configure the baud rate for the driver that transmits data to your device. Available rates are 57600, 115200, and 230400. The default rate is 57600.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal