DH+ Properties dialog box
How do I access the dialog box?
From the Explorer under the
FactoryTalk Linx
data server, double-click Communication Setup
, right-click the configured PKTX on DHPlus driver and then click Properties
.Use the dialog box to:
DH+
Properties - View and adjust the name of the driver
- Enter the Station Number for the driver
- View the Jumper ID
- Set the baud rate
Provide Feedback