Ethernet Properties, General tab
How do I access the dialog box?
From the Explorer under the
FactoryTalk Linx
data server, double-click Communication Setup
, right-click the configured Ethernet driver and then click Properties
.Use the
General
tab of the Ethernet Properties
dialog box to view or change the name of the Ethernet driver.Set other Ethernet driver properties on the
Advanced
tab.Provide Feedback