Ethernet Properties, Advanced tab
How do I access the dialog box?
From the Explorer under the
FactoryTalk Linx
data server, double-click Communication Setup
, right-click the configured Ethernet driver and then click Properties
.Use the
Advanced
tab of the Ethernet Properties
dialog box to:- Configure how the driver is exposed on the network. It applies only to workstations runningFactoryTalk Linx. On CE devices, these settings are ignored.
- Select the IP address of the Ethernet driver that will listen to data
- Select the MAC Address
- Enable or disable the Listen on EtherNet/IP encapsulated ports
Provide Feedback